VBUS.OVWTHRESH

Description

This parameter is the DC bus overvoltage warning threshold. When the measured DC bus voltage exceeds the threshold, an overvoltage warning is thrown.

Examples

Usage

The default value of VBUS.OVWTHRESH is 0, which turns the overvoltage warning off.

If this parameter is nonzero, the drive throws Warning 2006: Bus over voltage, when the measured DC bus voltage VBUS.VALUE is greater than VBUS.OVWTHRESH. It clears the warning when VBUS.VALUE drops below 97% of VBUS.OVWTHRESH.

Code

When VBUS.OVWTHRESH is set to 0, the drive does not report an overvoltage warning.

--> VBUS.OVWTHRESH
0 [Vdc]
--> VBUS.VALUE
403.723 [Vdc]
--> DRV.WARNINGS
No warnings active

Change the overvoltage warning level to a nonzero value. When the bus voltage is higher than this value, the overvoltage warning is reported on each axis.

--> VBUS.OVWTHRESH 400
--> VBUS.OVWTHRESH
400 [Vdc]
--> VBUS.VALUE
403.723 [Vdc]
--> DRV.WARNINGS
1-2006: Warning: Bus over voltage.
2-2006: Warning: Bus over voltage.

When the bus voltage drops below the VBUS.OVWTHRESH, but is still greater than 97% of the threshold, the warning persists.

--> VBUS.VALUE
394.272
--> DRV.WARNINGS
1-2006: Warning: Bus over voltage.
2-2006: Warning: Bus over voltage.

When the bus voltage drops below 97% of VBUS.OVWTHRESH, the warning is removed.

--> VBUS.VALUE
378.521
--> DRV.WARNINGS
No warnings active

Context

For more information on DC bus protection, see Power and Regeneration.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units Vdc
Range 0 to 900
Default Value 0 (warning disabled)
Data Type Integer
See Also VBUS.VALUE, VBUS.OVFTHRESH

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

VBUS.OVWTHRESH

300ah

08h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2508

1

2508 (0x9cc)

VBUS.OVWTHRESH

Unsigned16

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

VBUS.OVWTHRESH

2508

Unsigned16

Read/Write

-